Cancel
Showing results for 
Search instead for 
Did you mean: 

Dialog

Pioneer
Pioneer

Hello,

 

Is it possible to open the dialog when i open the model or run a method when opens the model.


Att,

2 REPLIES 2
Highlighted

Re: Dialog

Legend
Legend

Hello,

To show your dialog you can use the method Open.
This way : Youdialog.Open() ;

BR
O.C

Re: Dialog

Siemens Phenom Siemens Phenom
Siemens Phenom

You can create a method called "autoexec" in the class library. In this case Plant Simulaton will run this method when your model is loaded. From it you can open a dialog window or even minimize Plant Simulation to the tray using HideBBL operator and leave only dialog window on the screen.

Regards, Vladimir.