Cancel
Showing results for 
Search instead for 
Did you mean: 

Different mu's to different successors

Builder
Builder

Hello everyone,

             

  How to model in such a way that single source which produces MU's in two table files should go to different successors. for example Mu's in table file1 should go successor 1 then tablefile2 to successor 2. 

4 REPLIES 4

Re: Different mu's to different successors

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello gopi,

 

I do not get it. Normally a Source refers to a single TableFile only.

 

You can always use the (default) Cyclic exit strategy and turn on Blocking. Then it will alternate between the available successors. Or choose MU Attribute if it has to be based on specific MU attributes.

 


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Different mu's to different successors

Builder
Builder

Thanks for your reply.

If there are 10 MU's in a table file, then first 5 go to successor 1and remaining go to successor2. 

To do so, i have done this

in the exit strategy of the source --blocking--Mu attributes--integer--openlist--(Mu's 1-5;successor-1;mu's6-10;successor2)

but still all the Mu's going to successor 1 only.

 

could you help me please?

 

Re: Different mu's to different successors

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Ok, slight misunderstanding of this strategy. You need to indicate which attribute (e.g. Name) of the MU determines where it should go. If you give the first 5 a different name, then you can use that. to send them to the correct exit. So, Blocking=true, MU Atribute, Attribute type=string, and something meaningful in the list (e.g. row 1: Name, Green, 1, row 2: Red, 2, row 3: Blue, 3).

 

Or: use the Cyclic sequence and set 1,1,1,1,1,2,2,2,2,2 in the rows.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Different mu's to different successors

Builder
Builder

thank you very much.

it worked out.