Cancel
Showing results for 
Search instead for 
Did you mean: 

Different process time for the same MU and same station by method

Creator
Creator

Hello.

I have some process time in a table,one type MUs,two singleproc,

I want to use a method to control two singleproc'sprocessing time.

For example:

the first MU,Its processing time by two station is table[1,1]and[2,1],

the second MU,its processing time by two station is table[2,1]and table[2,2]...and so on.

I try to write the method,but I don't have enough ability to finish,hope somebody help me,

 

Thanks!

2019-04-25_105901.png

 

4 REPLIES 4

Re: Different process time for the same MU and same station by method

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi!

 

Rather than using the "List(Type)" option you can use the "Formula" option on the processing time. Then you can access the values by pointing to the correct cell in the table. Take a look at the attached picture and model.

ProcTimes.png

Re: Different process time for the same MU and same station by method

Creator
Creator

Thanks to MarcusA for your reply,

 

But the Simulation setup must create a new MUtype for a new set of processing parameters,

if I have thousands of processing parameters, I have to create the same number of MUs.

I hope I can do the simulations by one MU type

 

Thanks!

Re: Different process time for the same MU and same station by method

Siemens Phenom Siemens Phenom
Siemens Phenom

You could try to use '?.statNumIn' instead of '@.name' in the formula then. In that case the first MU that enters will get read the value from the first row, the second from the second row and the n:th from the n:th row

TimeTable[?.name,?.statNumIn]

Re: Different process time for the same MU and same station by method

Creator
Creator

Thanks to MarcusA for your reply,

 

This simulation setup is effective,

 

Thank you very much!