Cancel
Showing results for 
Search instead for 
Did you mean: 

Different processes by the same machine components

Experimenter
Experimenter

 

 

Hello, 

I have problems with modeling a machine.

I don't know how declare relations between different processes that get done by the same machine components.

For example: Process "Weld" and "Weld1" are done by the same Spot(weld)Gun, so they can not happen at the same time.

Or For example: all the movement between the processes are done by one the same handling robot, so they can not happen at the same time as well. 

Screenshot_2.png

 

 

the order in which the processes runs is as follows:


Screenshot_3.png

 

So my questions are;

How can I declare relations between different processes that get done by the same machine components?

How can I determine the order in which the processes runs?

 

I hope somebody can help me.

Thanks in advance.

 

RemcoW

2 REPLIES 2

Re: Different processes by the same machine components

Hi RemcoW,

you should have a look at the whole importer broker exporter mechanism.

A good starting point are the sample models.

 

With regards

Andreas

Broker.PNG

Betreff: Different processes by the same machine components

Phenom
Phenom

 

 

I've attached how stations can to share resources ( eg. robot) through an expoert object.

 

Please keep in mind that the robot now has only half the cycletime to accomplish a job at the station

 

Unbenannt.PNG