Cancel
Showing results for 
Search instead for 
Did you mean: 

Difficulty in writing/exporting table file into excel worksheet

Creator
Creator

Hello everyone,

 

I want to know any method which would write large data stored in the table file od excel into the excel file .

 

I tried using "writeexcelfile" command but is is taking lot of time 15-20 mins to write the data into designated excel file. I am writing a data which is of size say columns :- 200 and rows :- 20000

 

Does anyknow know any method to write into excel file quickly?

 

Thank you.

 

 

5 REPLIES 5

Re: Difficulty in writing/exporting table file into excel worksheet

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi GS,

 

you can use the 'writeFile' method of a table to write the data as comma seperated values (csv) top a text file.

 

This can be read by Excel and it is much faster.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Difficulty in writing/exporting table file into excel worksheet

Experimenter
Experimenter

Hello Ralf,

 

May I know on using "WriteFile" command, what delimiter is used when copying data to the .txt file.

 

I am finding trouble in copying the data from the .txt file to MS Excel using a macro which I developed as it is ignoring the "tabs" between the values and pasting them in excel in a single cell.

 

Thank you,

Yogesh

Re: Difficulty in writing/exporting table file into excel worksheet

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Yogesh,

You can define the seperator you want to use.

Open a table, select the List ribbon and then go to 'Export->Text File Format'. Here you can set the column seperator to a semi-colon.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Difficulty in writing/exporting table file into excel worksheet

Experimenter
Experimenter

Hey Ralf

 

It shows the default column separator as "Tab".

 

Will this hold true when I write the tables into a .txt file?

 

I am writing all my results tables in the endsim method to avoid saving manually each time.

 

Thank you,

Yogesh

Re: Difficulty in writing/exporting table file into excel worksheet

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, the seperator which is shown here will be used to write the table into a .txt file.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.