Cancel
Showing results for 
Search instead for 
Did you mean: 

Disable Inheritance in Chart

Pioneer
Pioneer

Dear all,

 

I'm currently struggling with deactivating the inheritance in the Dialog Window of a chart object.

I created a frame containing a chart. I create around 100 objects as children from that frame and place ParallelProcs in them (different buildings). The idea now was to use the chart in each frame to show the statistics of the ParallelProcs in the frame. However, each and every one of the InputChannels table of each chart in each frame refers back to the InputChannels table in the Parent Frame.

Does anyone know how to disable this specific inheritance via a method?

 

Best regards

 

Tim

5 REPLIES 5

Betreff: Disable Inheritance in Chart

Gears Phenom Gears Phenom
Gears Phenom

Hi Tim,

see here:

grafik.png

So basically, you just need to do this:

var t := Chart.InputChannels
Chart.InputChannels := t

Regards,
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Disable Inheritance in Chart

Pioneer
Pioneer

Hi Alex,

 

I can't believe I didn't see that - thank you so much!

 

Best regards

 

Tim

Re: Disable Inheritance in Chart

Valued Contributor
Valued Contributor

Hi, I'm also struggling with chart inhertance but my issue is with the Annotations table. The workaround here doesn't apply since there's no text field. Seems like a get/set method should exist. Please help!

Re: Disable Inheritance in Chart

Gears Phenom Gears Phenom
Gears Phenom

Edit: Sorry, wrong login the first time :-D

Well, I quickly checked it in PS14.0 and there is no issue with the inheritance. You can set/get the annotations-table like this:

var tab : table := Chart.Annotations
tab.writeRow(1,1, 2, 1, 1, 10, 5, 0, "Hallo")
Chart.Annotations := tab

I hope this helps Smiley Happy
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Re: Disable Inheritance in Chart

Valued Contributor
Valued Contributor

Thanks Alex. Simply using ":=" did the trick.