Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Display panel doesn't update the values

Legend
Legend

Hello everyone, 

 

I just installed the last version 12.2 and I noticed that the display panel (shows StatunumIn) doesn't update the values automatically. In order to make the display panel shows the right value I should stop the model. And when I start the model anew the display panel value still blocked on the previous value. No way to see how the value is changing during the calculation.

 

Thank you very much for your help if anyone have an idea.

BR
O.C 

2 REPLIES 2

Re: Display panel doesn't update the values

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello ocsim56,

 

did you activate your display panel? If you do not see the number, may be the number is outside the frame.

Attached you will find a small demo model with dispay panel activated.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: Display panel doesn't update the values

Legend
Legend
Hello GG,

Thank you for your reply. The display was activated and the number was inside the frame.
I think it was a beug on my computer. I closed and opened the model this morning and it works well.

I hope it will not happen again !
Thank you GG.

BR
Omar