Cancel
Showing results for 
Search instead for 
Did you mean: 

Drag and Drop Shift Calendar

Legend
Legend

Hi! 

 

I want to use the same shift calendar for all elements in my model.

 

When I select all the elements and drag-drop them on the Shift calendar, the names are added in the resources. But, it does not apply to the objects which are in sub-frames.

So, apparently the subframes do not have any unplanned or paused times.

 

Am I doing something wrong?

 

Also, is there an easier way to  do this instead of going into each subframe and specifying/drag-drop to the shift calendar in the root?

 

Sanchay

4 REPLIES 4

Re: Drag and Drop Shift Calendar

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
you can define the shift calendar once for each type of station in the class library. tab controls:

root.ShiftCalendar
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Drag and Drop Shift Calendar

Legend
Legend

Thanks. I was trying to avoid that because I was planning to have duplicate frames operating on different shift calendars.

 

But, if nothing else can be done, I will eventually do what you told in different model files.

 

Thanks again..

Sanchay

Re: Drag and Drop Shift Calendar

Phenom
Phenom

You could set the shiftCalendar in the class objects.

It should then be automatically linked when drag & dropping the the objects/subframes into the root frame

containing the shiftCalendar.


Or you could use the AttributeExplorer to select and set the objects shiftCalendar attribute



Re: Drag and Drop Shift Calendar

Legend
Legend

@simulator wrote:
You could set the shiftCalendar in the root objects.

It should then be automaticlly linked when drag & dropping the the objects/subframes into to the root frame

containing the shiftCalendar.

I will definitely do this when I'm making a new model next time. Now that the model is almost ready, it seems that it does not make a difference.

 

On the other hand, the attribute explorer seems much more convenient at this time.

Thanks a lot.