Cancel
Showing results for 
Search instead for 
Did you mean: 

Drain Statistics

When one selects a Drain object in a model, after the model has executed, and one presses F6, many statistics are displayed, also of MUs that passed through the Drain. However, when I select a Drain object and press F8, I only see the watchable drain statistics. How can one access the many useful MU statistics?

2 REPLIES 2

Betreff: Drain Statistics

Gears Phenom Gears Phenom
Gears Phenom

Hi Simulationist,

 

I cannot reproduce your problem. When I press F8 it displays all attributes of the drain, maybe you changed some of the filter settings in the attribute-window?

 

When you look at the Drain dialog, go to the tab with the type-specific statistics, there you can also see the statistics from the F6-window. Now you can click the "question mark" in the upper right corner and click on any of the statistics-values; a popup will show that also tells you the attribute-name.

 

For example the MUs that passed through the drain:

  • in total: statDeleted
  • per hour: statThroughputPerHour
  • per day: statThroughputPerDay

 

Regards,

Alex

 

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Drain Statistics

Alex, the F8 feature is exactly what I was looking for. Thanks a lot.