Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

EXIT FROM A LINE WHEN A CONDITION IS TRUE

Pioneer
Pioneer

Hi guys,

I think that my question is super easy but I can't understand why my exit strategy is not working.

If you look the picture Cattura1 you can see the easy example I am working with. 

What I want to obtain is a control of the red line that allow the entities move in the next line (blue) only if in the yellow line there are not packages.

 

What I did is an exit strategy (Cattura) on the red line based on the MUAttribute "NumMU) of the yellow line.  If there are some packages in the yellow line (Line2) i want to stop my packages in the red line (Line)

Thanks in advance for your  help,

Diego

1 REPLY 1

Re: EXIT FROM A LINE WHEN A CONDITION IS TRUE

Phenom
Phenom

Generally this exit strategy is based on the 

 

attributes of the triggering MU on the red line and

 

not on any other attributes ( e.g. ones of  the other yellow line).

 

To get your model working as intended, use a waituntil statement

 

in the exit control of the red line.