Cancel
Showing results for 
Search instead for 
Did you mean: 

Editing a method in a separate window.

Valued Contributor
Valued Contributor

Hello, is it possible to edit a method in a separate window similarly to how it appears when there is an error in the code during a running simulation?

 

Generally when editing a method it kicks me into a different tab, and I can't see my model. It would be much easier if I could easily access the method in a separate window so that I could edit it while still having visual access to my model.

 

Thank you

2 REPLIES

Re: Editing a method in a separate window.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello mbuschur,

 

no, this is not possible. The debugger window is a dialog, unlike the method windows.

 

You could use the 'Tile Vertically' command from the Windows ribbon.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Editing a method in a separate window.

Valued Contributor
Valued Contributor
Not quite what I was looking for, but that will work well enough. Thank you!