Cancel
Showing results for 
Search instead for 
Did you mean: 

Entrance gate

Pioneer
Pioneer

What's the difference beetween set up time and recovery time?

 

For example, in my case, if a machine is paused I want to program the time that occurs till is attivated to work to really start processing MU.

 

Thanks.

 

Best regards,

 

João

1 REPLY 1
Highlighted

Re: Entrance gate

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi João,

 

Setup time is consumed when the part type changes or a certain number of parts are processed.

It's the time before processing is started.

 

Recovery time is consumed after each part and defines the time until the next part can enter.

 

So in your case you should be able to use setup time with a setup required after each part.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.