Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Equip SingleProc

Valued Contributor
Valued Contributor

Unbenannt.PNG

Hey,

 

Okay the loop makes sense but what I don't understand is why my value is "red"? The value is the time I need to equip my SingleProc.

 

I have a list transformed from the Source like you can see at the pic. I gave the columns the following values:

Number is the rate

Name is the name of my container

Attribute is the color

 

So in the sublist I need the specification that the Attribute is the deciding equip attribute color and the value to equip of one minute. That means that the program actually does not contain the time value.

 

Maybe that's why all of this makes no sense. Because the list I give the program contains these 3 values and the SingleProc should equip when the Color changes and this takes 1 minute.

 

So for me this code is not really helpful I think.

Or do I understand wrong?

Highlighted

Re: Equip SingleProc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

okay, to make it complete: if you want to have a second user defined attribute with the name e.g. equiptime, datatype time, value one minute (or color based), you need to extend the program:

 

for var i:=1 to main.yDim loop
  Main.erzeugeSubliste(4,i); //creating a sublist at the mainlist
  Main[4,i] [1,1] := "Color"; //name of the Attribute
  Main[4,i] [4,1] := "red";//value in column "string"
  Main[4,i] [1,2] := "equiptime"; //name of the Attribute
  Main[4,i] [6,2] := 60;//value in column "time"
next

Insead of red and one minute insert your data from your table. If you mean with "equip" setup and if the setup time is constant, you dont need a user defined attribute, you only need to insert the setup time in the field setup time in your machine.

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Equip SingleProc

Valued Contributor
Valued Contributor

Okay I understand that's the reason why I don't need the time. Now it's clear thank you!

 

But anyway the code is still not working... Do I have to connect the method somehow to my List?

As I know normally it should work automatic.

 

I have a List called Main

my columns are called

MU(object) - Number(integer) - Name(string) - Attribute(table)

and than I just filled in my values and wrote the method but a sublist is not created and also not filled up...

 

What did I forget?

 

 

Also I tried to modify the code. Because I already have the color at the attribute column, so I just can copy the name:

 

for var i:=1 to main.yDim loop
  Main.erzeugeSubliste(4,i); 
  Main[4,i] [1,1] := "Color"; 
  Main[4,i] [4,1] := Main(4,i);
next

 

but its not working as well...

Re: Equip SingleProc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you need to start the method (e.g. right mouse click on the method --> run) Where do you have the colors for the lines of the main table? You need square brackets to access the table...

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Equip SingleProc

Valued Contributor
Valued Contributor

Good morning,

 

now its working but its doing something really strange...

 

At the beginning I have my original table (see Pic1) after running the method all my colors disappear (see Pic2)...

So I think that something in my code is still wrong I think because in the sublist its not writing down the name from the table its just writing main[4,i](see Pic3)...

 

Thats my code at the moment:

 

for var i:=1 to main.yDim loop
  main.erzeugeSubliste(4,i); 
  main[4,i] [1,1] := "Color";
  main[4,i] [4,1] := "main[4,i]"
next

 

Pic1.PNGPic2.PNGPic3.PNG

Re: Equip SingleProc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
when you create a subtable, the content of the cell will be replaced, this is the default behavior.
Enter the colors in column 5 (change the maxXDim attribute of the table in the attributes and methods dialog)

then try this
for var i:=1 to main.yDim loop
main.erzeugeSubliste(4,i);
main[4,i] [1,1] := "Color";
main[4,i] [4,1] :=main[5,i]
next
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Equip SingleProc

Valued Contributor
Valued Contributor

I inserted the 5th column.

 

But now its getting really strange...

If I use one of these codes its not working:

 

main[4,i] [4,1] := main[4,i];

main[4,i] [4,1] := main[5,i];

 

But if I use this one its working perfectly:

 

main[4,i] [4,1] := main[3,i]

 

Do you know why?

Re: Equip SingleProc

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
can you send me your model?
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Equip SingleProc

Valued Contributor
Valued Contributor
I already solved it!
I had the wrong datatype...

The model is now working very well.
Thank you for your time and your help!

Best regards,
IceTea