Cancel
Showing results for 
Search instead for 
Did you mean: 

Error Message : Run Time Error Occured

Creator
Creator

Hi,

 

This message (see photo below) comes every time I try to save my model after running it. It seems like it is caused from when I select "None" in 3D Preferences --> Graphics --> Obstacle for Workers. Without this the workers wont be able to move around in my frame at all, so I am forced to use this setting. 

 

I have tried to choose (after suggestions in another discussion thread in this Forum) a lower OpenGL level in the preference dialog under File --> Help --> Preferences. I tried with all levels, but non of them are working.

 

Also, I tried to open the program on different computers with different graphic drivers.

 

Are there any other suggestions from you guys that might help me with this problem?

 

Cheers,

Mal

 

1 REPLY 1
Highlighted

Re: Error Message : Run Time Error Occured

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you post the model so that I can investigate the crash?

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.