Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Error/Problem with Kanban (Value Stream Mapping)

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Irina,

 

the latest patch for V11 is 11.0.9.

 

You can download it here: https://download.industrysoftware.automation.siemens.com/tecnomatix/Plant_Simulation/Patches/Version...

 

For 64-bit you need the file PlantSimulation11.0.9.64bit.Software.exe.

 

You can also start Plant Simulation. The go to the Help menu and choose "Online Technical Support->Download Latest Product Updates". Then you will be directed to the right download location.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Error/Problem with Kanban (Value Stream Mapping)

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Thanks, Ralf. We well try to go via help> support > download.

 

Still, just to clarify - we cannot go to version 12 if we have version 11 installed?

 

How do I know which one is PlantSimulation11.0.9.64bit.Software.exe from the screenshot below? Thanks

Updates.jpg

Re: Error/Problem with Kanban (Value Stream Mapping)

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Irina,

 

you can install V12 in parallel to V11. Then you can use both versions as appropriate.

 

You cannot download the setup for 11.0.9. The setup for V11 is based on patch 3 I guess.

 

So you have to download the setup for V11 (Plant_Simulation_11_Setup_32bit_PCmsi or the 64bit version from the 64-bit folder).

Then you have to download the patch 11.0.9 and apply it to your installation.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.