Cancel
Showing results for 
Search instead for 
Did you mean: 

Error in dEmp with table

Pioneer
Pioneer

Good morning, I am using the dEmp funtion (with a table with the values) for change the time when a supplier send me the parts in order to simulate the possible delays in the shipping. The problem is that I have changed the values in the table but when I simulate last values continue appearing as it's possible to see in the photo:

fail dEmp.png

 

I have deleted the 15:12:00:00 time in the table and when I restart the simulation it continues appearing as it was still in the table. Anyone knows what is happening?

 

Besides,in the hole results table only appear 2 times and not the other 8 times. Any idea?

 

Thank you 

2 REPLIES 2

Re: Error in dEmp with table

Phenom
Phenom
what has the right table to do with the left table ?

which object writes the values into the right table ?

It would simplify understanding if you could provide that part of the model

which you think that doesn't work.

Re: Error in dEmp with table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the right is a timesequence, the content will not be deleted automatically at the start of the simulation, you need to do this by your own (e.g. init method--> Recording_plazos.delete)
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net