Cancel
Showing results for 
Search instead for 
Did you mean: 

Examples with PlantSimulation

Builder
Builder

Hi!

 

Is it too much effort to ensure, that the examples provided with PlantSimulation are kept up-to-date when a new patch level is released?

 

I have just opened a 3D demo model and PlantSimulation 10.1.11 reported a certain amount of outdated libraries. My experience with other discrete-event simulation programs were, that an update to the latest release does NOT always keep the examples stable.

 

Thx!

 

Mak

1 REPLY

Re: Examples with PlantSimulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Mak,

 

the examples run just fine with the old libraries, since they were tested with these libraries.

 

So there is no need to update our examples to the latest version.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.