Cancel
Showing results for 
Search instead for 
Did you mean: 

Exit control trigger on new shift start.

Valued Contributor
Valued Contributor

Hi,

 

I just spent a while debugging a model that worked perfectly fine until I added shifts on certain machines. This caused the Exit Control to trigger, decrementing a value for the amount of products of a certain type that need to be processed on that machine (a CNC machine that cuts plates and that I represented by a dismantleStation). Since this happened when the buffer after the dismantleStation was full and could not accept any more MUs, the value was wrongly decremented.

 

I can easily fix this by only decrementing the value only when the move method is succesful, but I am wondering:

 

- Why does this cause the Exit Control to trigger again?

- Is there any way to prevent this behaviour from occuring?

 

Many thanks in advance.

 

Kind regards,

 

Kaspar

6 REPLIES 6

Re: Exit control trigger on new shift start.

Phenom
Phenom

have you checked this setting ?

 

 

Unbenannt.png

Re: Exit control trigger on new shift start.

Valued Contributor
Valued Contributor

Hi,

 

Yes, I had that box checked, so I'm a little bit unclear as to why it triggers multiple times. If I have time I will try to make a small model to reproduce this situation, unless someone can answer me before that...

Re: Exit control trigger on new shift start.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

Did you find a solution? I have the very same problem now, a exit control in a parallellstation is triggered multiple times for the same MU, when a shift starts. 

 

How do you check if the .move is successful? How does it help you in the workaround?

Re: Exit control trigger on new shift start.

Valued Contributor
Valued Contributor

I met the same problem too, I think it maybe caused by that  the mu  in satation "A" did not enter the next station because  the next station is blocked in the end of a shift,   when a  new ShiftCalendar start it will  trigger the exit method again.   the  ways of resolution   may  like this ,in station ""A" define a Variable that record the mu which try exit the...Variable record   )  ,if yes  then we can  quit the exit method  use the code "return"

 

Re: Exit control trigger on new shift start.

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

It's probably like you say. What I don't understand is why it happens with the parallellproc, I don't have the same problem with singleprocs. I had a similar workaround like the one you mentioned, but the issue was that in the production the different products circulate between different machines (kind of lika a job-shop), so one product should be able to be in the same machine several times in a row. This makes the condition for when to return quite tricky, so I was hoping there was some easier way  to check it.

 

However, this is not really a problem anymore since I have changed the parallellproc to singleprocs instead. I have not run into any similar problems yet.

Re: Exit control trigger on new shift start.

Valued Contributor
Valued Contributor

Since <some MU>.move returns a boolean value, the best workaround for me was to check whether it actually moved on to its successor with if @.move and take appropriate action when it hadn't.