Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Exit count is more than entry

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Capture.PNG Hello,

 

Hello,

 

 what might be the reason for this ?

entry count -424

exit- 425

 

I have checked all the connections. deleted them and connected once again. tried it again but same result was there.

 

need help for resolving this.

 

Thanks in advance 

3 REPLIES

Betreff: Exit count is more than entry

Genius
Genius
I think it is after statistic reset and when statistic reset was, there was one MU on the station and now the station is empty.
__________________________________
Have a look in the help before asking.
EDAG-PS: https://www.edag-ps.de/

Betreff: Exit count is more than entry

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Yes,  I reset the statistic. what is to be done to correct it?

Betreff: Exit count is more than entry

Genius
Genius
Is it really important?
If you really want to correct it, you have to remember the numMu of the station while statisticreset. If you want to calculate sth. it is a possibility to use own variables,which won't reset during statisticReset.
__________________________________
Have a look in the help before asking.
EDAG-PS: https://www.edag-ps.de/