Cancel
Showing results for 
Search instead for 
Did you mean: 

Experiement Manager start and reset

Legend
Legend

Hello,

 

I would like to execute a method just before all experience (distributed or not). Maybe onClic "start" 

 

I know that there is a method executed after all experience and run : "Evaluation method". Is there the same for the very beginning ? Or a workarround ?

 

Best regard,

 

rpinon

6 REPLIES

Re: Experiement Manager start and reset

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
in the experiment manager: Tools - Advanced settings - Configuration method
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Experiement Manager start and reset

Legend
Legend

No for me configuration method start before each experiement.

Re: Experiement Manager start and reset

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

in this case you could also create an "init" method in your frame, as such it is called before each simulation run. Would that work for you?

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Experiement Manager start and reset

Legend
Legend

No I want a method this is called one time. At the very beggining of the experiement. (Evaluation do that for the very end)

Re: Experiement Manager start and reset

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Rpinon,

an experiment corresponds to a model parameterization.

If you have a distributed simulation, all parameters must be set on the remote Plant Simulation process.

Since the sequence of simulation runs is generally unpredictable, the configuration method must be called for each simulation run in case of a distributed simulation.

What do you say about this idea? You start the simulation study by a method:

YourMethod
Experimentmanager.resetWizard
Experimentmanager.Start

Regards,

Peter

Re: Experiement Manager start and reset

Legend
Legend

Hello,

 

Yes it is exactly what I do now.

 

But it's too bad that it is not integrated in the experiment Manager. Now i can't use the Experiment Manager's start button.

 

Thanks for reply.