Cancel
Showing results for 
Search instead for 
Did you mean: 

Experimenting with quantity of a type of machine as input variable

Pioneer
Pioneer

What is the most default way (involving least custom implementation) that I can adjust the quantity of a type of machine (in a location)?

 

For example, if I want to use this quantity in the experiment manager, how can I set it as an input variable?

 

I thought of using a parallelproc and adjusting the x or y dimension, but if the activity needs individual services (like workers) then this does not work because these apply to the proc. 

 

Thanks in advance!

 

 

5 REPLIES 5

Re: Experimenting with quantity of a type of machine as input variable

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

What you could do, is create individual objects in a script, based on a variable. Basically, you need to use two commands: createObject and connect. It is also wise to register the thus created objects in a table, so that you can easily delete them.

 

Here is a code snippet:

for i:=1 to NumberOfObjects loop
	obj:=.MaterialFlow.SingleProc.createObject(current,i*20,0)
	.MaterialFlow.Connector.connect(MyInfeed,obj)
	.MaterialFlow.Connector.connect(obj,MyOutfeed)
	MyObjectsTable.appendRow(obj);
next

Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com

Re: Experimenting with quantity of a type of machine as input variable

Pioneer
Pioneer

Thank you for your answer.

 

I thought about this approach, but I hoped that there was a default feature to replicate a proccessor 'in place'. I will accept this answer soon unless someone else can achieve this without code.

Re: Experimenting with quantity of a type of machine as input variable

Phenom
Phenom

Another way to scale the performance of  station using the eM

 

The easiest way is probably to scale/reduce the cycletime of the station.

 

 

Unbenannt.png

Re: Experimenting with quantity of a type of machine as input variable

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Actually, there is a second option.

 

You could create a model with the maximum amount of SingleProcs or other objects at the outset. In the ExperimentManager you should then disable one or more of these objects (e.g. set EntranceLocked=true). No code required, just the "maxmimum" model.


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com

Re: Experimenting with quantity of a type of machine as input variable

Pioneer
Pioneer

Thank you both for taking the time to respond to my question.

 

simulator, Im not sure about the accuracy of scaling the cycle time and the concern about services that I mentioned, and I cant see it happening in the model you attached.

 

In summary, it seem like there is no elegant way to achieve this, but the two alternatives proposed by Nomden will both work.