Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Export As JT - Frames

Phenom
Phenom

Hello

 

Thank you for the information, was trying to read up about the JT file format after making my post (to see about making a post export comparer or something) and could not even find if it included a time stamp or not.

 

You have given me quite a few ideas as to what I could try to do, sure dumping out some extra information about the 3D graphic will not be to hard, guess I could also possible dump out the graphic tree as well so I will be able to monitor that for any changes (incase some of the graphics are rearranged). Might need to experment about materials and see if changing the material has a large effect on the other attributes or not.

 

Lots of stuff for me to now try to do, but this can all wait until after Christmas. Thank you again.

 

JamesM

Re: Export As JT - Frames

Phenom
Phenom

Hello

 

Have now got around to carrying on with this and have got most of it work now by dumping out data at the same time as when i save the 3D model and then when going to save it externally I check the data against the model to see if anything has changed.

 

Have added in a few extra stuff, mostly saving the position, rotations and scale of the different graphics but i cannot find a way to check for the material. Through testing this might be an issue as only enabling the graphic material has a affect large enough for me to detect and not changing a material that is already applied.

 

Is it possible to get the material of a graphic through simtalk?

 

JamesM

Re: Export As JT - Frames

Siemens Phenom Siemens Phenom
Siemens Phenom

I'm afraid that there is currently no way to read a material of a graphic via SimTalk.

For object materials on MUs, workers and stores, this is possible, but as of now, not for graphics.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: Export As JT - Frames

Phenom
Phenom

Hello

 

Ok, thank you for your help on getting this done.

 

As a side note, did find the memory used quite strange as during testing it was not changing at all, then i closed and reopened the model and it started to change a bit (so have added a 10% tollerance when checking, yes i know even less chance of finding the change for materials).

 

JamesM

Re: Export As JT - Frames

Experimenter
Experimenter
Hello

Can you help me with graphic of MUs object, how can I change it if I have .jt model?

Thank you

Re: Export As JT - Frames

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
open the MU in the class library in 3D,klick on the 3D header, select edit - Import Graphics
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Highlighted

Re: Export As JT - Frames

Experimenter
Experimenter
I know that I can change graphic of Sourse or SingleProc, but I cant to do it with MUs as you see Programme on Russian, as you see I don't have this batton

Re: Export As JT - Frames

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
it should be on the tab правка
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Export As JT - Frames

Experimenter
Experimenter
Thank you so much!

Re: Export As JT - Frames

Experimenter
Experimenter

Hello

 

Exuce me, can you advice me some material for Plant Simulation learning. I want that it will be the most effectivly.

 

Thank you!