Cancel
Showing results for 
Search instead for 
Did you mean: 

Flow of elements through selected workstations - problem

Experimenter
Experimenter

I have a problem. How to create a table and how to control the flow of elements through given workstations? Attached is my model, which I have prepared so far.

2 REPLIES

Betreff: Flow of elements through selected workstations - problem

Gears Phenom Gears Phenom
Gears Phenom

You only need to process the parts on a subset of stations, but the materialflow always goes through all of them, right? So e.g. "TypeA" is not processed on Stanowisko2..5, but still moves through them, right?

You also need a table with the processing time on each station, because you have to dis/enable that for each MU. Create an EntranceCtrl ("before actions"!!!) for the SingleProc (do it for the class-object, so you only need to do it once) like this:

-- (de)activate processing-importer according to workplan
TypeProcess.setCursor(@.Name, 1)
?.ImporterActive := TypeProcess.find({@.Name, *}, to_str("WP_", ?.Name))
if ?.ImporterActive then
	?.ProcTime := 60 --> replace this with the actual time of each station that you need!!!
else
	?.ProcTime := 0
end

grafik.png

Regards,
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: Flow of elements through selected workstations - problem

Experimenter
Experimenter

That's it! Thank You very much!