Cancel
Showing results for 
Search instead for 
Did you mean: 

FlowControl exit strategy

Genius
Genius

Hello everybody,

     

I wonder how it is possible to control the exit of a "flow control" stating how many entities should be sent to each successor.
For example, I would have the firsts 30 MU arriving to be sent to the successor 1, the next 20 to 2 and at the end the cycle is repeated.
Attached is a model that does the above exemple using the strategy "Cyclic sequence", but when the numbers became very large  the table is difficult to be filled.

 

 

Thank you for your help

2 REPLIES

Re: FlowControl exit strategy

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you could use a table to count the MUs and to switch between the exits.

 

flowControl.png

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: FlowControl exit strategy

Genius
Genius

Hello Steve,

 

I was hoping there was a native functionality on the software, but your solution certainly solves the problem.

 

 

Thank you for your help