Cancel
Showing results for 
Search instead for 
Did you mean: 

Funny error message in the code editor

Legend
Legend

Hello everyone,

 

I just missed clicking on a button in the code editor, and that showed me an error message saying "Invalid parameter" or some such. It was shown in my native language. I've attached a model showing the error.

 

You need to click where shown in the image for the error message to appear. It only shows when both scroll bars are active.

1 REPLY

Re: Funny error message in the code editor

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Verbalins,

 

this issue will be fixed in the first maintenance pack (12.2.1) for version 12.2, which will be released within the next few days.

 

Thanks for reporting this issue!

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.