Cancel
Showing results for 
Search instead for 
Did you mean: 

Generating MUs using information of a table's second and third column

Pioneer
Pioneer

Hello all,

I have problems figuring out how to solve the following problem concerning using a table.

I would like to create MUs using a table (Production) (that isn’t a problem). But at the same time I would like to look up in another table (Planning) which other MUs I have to create in the processes before (basically in a second and third column). Thus, the MU has to wait at the source until the other ones have been produced, respectively moved (c.p. method). I included a specific attribute, that's why I only used Strings in the table "Planning".

I would appreciate any kind of help. Thank you.

Regards,

David

 

  

2 REPLIES 2

Betreff: Generating MUs using information of a table's second and third column

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello David,

 

I attached your model with some modifications. in the exit control of the source, the additional products are first created before the main product will be moved on to the buffer.

 

Hope this will help you.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Generating MUs using information of a table's second and third column

Pioneer
Pioneer
Hello GG,

Thank you for taking the time and looking into it. I would like to look into your modifications, but unfortunately it seems like the attached file is the same as the one I uploaded. At least, I cannot see any exit control.
Would you be so kind and ulpoad your revised version one more time please?
Thank you,
David