Cancel
Showing results for 
Search instead for 
Did you mean: 

Geometry culling

Creator
Creator

Is there any way of turning off geometry culling in 3D so that when you zoom out your mus don't disappear?

 

Thanks.

5 REPLIES 5

Re: Geometry culling

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

you can adjust that by clicking on the "File" ribbon, there you select "Model Settings" and in the tab "3D" you have to set the "Screen coverage threshold" to zero. 

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Geometry culling

Creator
Creator

Unfortunately already tried that and it made no difference:

 

Zoomed In:

ZoomedIn.PNG

 

Zoomed Out

ZoomedOut.PNG

 

Any other ideas?

Re: Geometry culling

Phenom
Phenom

The MUs probably have multiple level(s) of detail (LOD).

 

Maybe you can delete the ones which are not fully displaying all MU details

 

Have a look at the 3d structure of your class MU and check and then delete the LOD.

 

Backup/ Duplicate the Mu before you start deleting any LOD !

Re: Geometry culling

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

what you can do in this case is to open the 3D Graphic of the class of your custom object in a new 3D window. For that you right click on your custom object in the Class Library and choose "Open in 3D". There you right click on it and choose "Optimize". Here you click on "Preview Result" and if the result is acceptable afterwards on "Accept Result". Afterwards this problem should be fixed, but if that issue is still persisting could you post your 3D object here?

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Geometry culling

Creator
Creator

That's resolved my problem, thank you.