Cancel
Showing results for 
Search instead for 
Did you mean: 

Getting the click location of a Button

Phenom
Phenom

Hello all.

 

Is it possible to get out the location clicked on a button or another object without having to cut up your object into multiple objects.

 

For example if I had a button could it be possible to know the coordinates of where on that button has been clicked so it can be used as part of a method?

 

JamesM

2 REPLIES 2

Re: Getting the click location of a Button

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello James,

 

sorry, but this is not possible.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
Highlighted

Re: Getting the click location of a Button

Phenom
Phenom

Hello.

 

Thank you, was thinking this was the case but thought I would ask here quickly just to make sure I was not missing something.

 

JamesM