Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

HBW

Creator
Creator

Can anyone help me with step by step modelling a HBW model

4 REPLIES 4

Re: HBW

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

2D or 3D ?

Do you want to use the HBW-Library of Plant Simulation?

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: HBW

Creator
Creator

i have HBW-Library of Plant Simulation with me.

 

i need step by step instructions to set up a model using HBW.

Re: HBW

Creator
Creator

I have HBW-Library of Plant Simulation with me.

 

I need step by step instructions to set up a model using HBW.

Re: HBW

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

what could help in this case is also to have a look in the example collection, there you find under "Small Examples" two models of implemented HBWs. You can also find additional information regarding the HWB in the Plan Simulation help when searching for "HBW".

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution