Cancel
Showing results for 
Search instead for 
Did you mean: 

Help Fixed using the other singleproc in the route

Valued Contributor
Valued Contributor

hello,

 

I have been trying to create a small process. Where I have two main processing machine (1.(schaum1+schaum1fertig), 2.(F2+FF2)). they both do the same work, so according to my model: the parts should go there simultaneously via transporter and finish it cycle time and go back to drain. But due to sensor position, only the first F2 is getting all the parts and Schaum1 stays empty all the time. (ideally, they both should work simultaneously).

rules are transporter can carry only one part at a time and the parts should wait before assembly and not at transferstation.

 

but main thing, i want the other schaum1 station to be working simultaneously.

 

thanks in advance.

2 REPLIES 2

Re: Help Fixed using the other singleproc in the route

Legend
Legend

Hi,
for example you can use destination in MU.

 

Destination.jpgexample

 

 

Regards
Nadin

Re: Help Fixed using the other singleproc in the route

Valued Contributor
Valued Contributor
Hey Nadin,
It works fine. Thanks Smiley Happy