Cancel
Showing results for 
Search instead for 
Did you mean: 

Help with Transfer station

Pioneer
Pioneer

Hello, 

i'm starting to develop a test model and i'm using a transfer station to load products onto transporters and another transfer station to unload them onto a drain. For that i have a sensor for the first TS to load and another for the second one to unload. 

The problem is, the second transporter only leaves the sensor when the first one arrives on it's target, but i want it to move right behind the first one. I don't want a gap between two transporters, i want (as long as there is a product ready for transportation) the transponter to leave right away, even if the previous one hasn't arrived yet.

 

3 REPLIES 3
Highlighted

Re: Help with Transfer station

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can you post your model?

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Help with Transfer station

Pioneer
Pioneer

Yes i can, thanks for the reply.

Re: Help with Transfer station

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

the green LED ontop of the transferstation means, that the transferstation is working (loading). If you want to start earlier with the transporter, you need to change the time in the transferstation and in the PlaceBuffer. The same for unloading.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net