Cancel
Showing results for 
Search instead for 
Did you mean: 

How can I modify the thickness of the LineSet ?

Legend
Legend

Hello everyone

 

I'm trying to build a dynamic rack by Simtalk in 3D view. 

I'm using the method "createIndexedLineSet" it allowed me to create a line in 3D. But I would like to modify the thickness of that line. Does anybody know how can I do that ?

Thank you very much. 
O.C

2 REPLIES

Re: How can I modify the thickness of the LineSet ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Omar,

 

there is no way to modify the thickness of the lines. These are really just lines.

If you want to build graphics such as racks, it might be better to use createIndexedFaceSet instead.

 

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: How can I modify the thickness of the LineSet ?

Legend
Legend
Hello Peter,

Thank you very much for your answer.
I used to use createIndexedFaceSet but I prefered LineSet with the Shadows it makes the automated storage more realistic. With createIndexedFaceSet it was hard to see what's happened on the cells with a huge storage.
But it's okay ! Thank you very Peter.
Take care.

Omar