Cancel
Showing results for 
Search instead for 
Did you mean: 

How do I limit total processing time on a parallel processing station?

Experimenter
Experimenter

My problem consists of 2 parts.

 

1. How do I keep track of the total processing time of a parallel processing station?

Where the Parallel station can process 4 different MUs at a given time, within a model with 4 MUs which each have a unique processing time. 

 

2. How do I limit the capacity of the parallel processing station?

For example, the simulation runs for 1 hour, and in that time the maximum processing capacity of the station is 3 hours.  3 MUs enter the station, each with a processing time of 1 hour. How do I stop a 4th MU to enter the station, until there is capacity again?

 

 

1 REPLY 1

Re: How do I limit total processing time on a parallel processing station?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

1. have a look in the statistics of the ParallelProc --> statWorkingTime

 

2. see help xDim, yDim

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net