Cancel
Showing results for 
Search instead for 
Did you mean: 

How o use Stat:Fit at the Plant Simulation

Creator
Creator

Hello dears.
I used the stat::fit to estimate the relevant distribution fit of the data of a table (times of production) and I would like to use this on the Plant Simulation (Processing time of a SingleProc - Lognorm).
Can I to do it? In attached you can see the distribuition with Stat:Fit.
Thanks!

4 REPLIES 4

Re: How o use Stat:Fit at the Plant Simulation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

just select lognorm infront of the textfield of the ProcTime and enter your parameters separated by comma like shown in the dialog

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Highlighted

Re: How o use Stat:Fit at the Plant Simulation

Hi Prieto,

just in case you are new to Plant Simulation:
You can also use emprical distributions for the processing time of a station (see exampe with cEmp in screenshot). In your case the lognormal distribution doesn't seem to fit your data very well, so perhaps an empirical distribution is the better choice.

 

cEmp.PNG

Re: How o use Stat:Fit at the Plant Simulation

Creator
Creator

Hi Steffen.
Ok, but it isn't works. First, how the MU is < 0, an error message window is shows, second, if the MU are positive number, an error message window is shows about the value exceed. I don't can write the distributuion parameters on the textfield.

Re: How o use Stat:Fit at the Plant Simulation

Creator
Creator


Hi Andreas,
Thanks. Yes, I am new to Plant Simulation, but I liked your idea. I will  leave it as plan B.
Note: the distributions are aleatory sample, don't are real. The real distribution look a lognormal (processing time).