Cancel
Showing results for 
Search instead for 
Did you mean: 

How to assigne a user defined attribute for all the MUs in one batch?

Valued Contributor
Valued Contributor

Hi:

 

I tried to assign a Batch number for each batch. So when this batch is in production, I know this is Batch No.24 ( for example) and next Batch will be No.25. We have two part models -- 50T and 675T, we run one batch then switch to the other model batch. If we run 50T first, then all the batches for 50T are odd numbers (1,3,5,7 ....), and the batches for 675T are even numbers(2,4,6,....).

 

I used Assembly machine, and container to pull a batch. Then use DismantleStation to deliver MUs to the conveyor.

 

What is the best way to put Batch Sequence number on each MU?

 

Thanks

Steve

7 REPLIES 7

Betreff: How to assigne a user defined attribute for all the MUs in one batch?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello GM_Lin,

 

add an attribute 'BatchNumber' of type integer to your class object of your MUs. At the assembly station you also add a variable of type inter as global batch number. Assign the global batch number to the batch you crreated on the assembly station. As soon as the container leaves the Assembly, increment the global batch number. 

Hope this helps.

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: How to assigne a user defined attribute for all the MUs in one batch?

Valued Contributor
Valued Contributor

I attached a small model. I still couldn't make it happen. The problem is how to assign the Global Variable: Batch_var, to the MU's attribue BatchN at the dismentalstation. Please help.

 

Thank you.

Steve

Betreff: How to assigne a user defined attribute for all the MUs in one batch?

Phenom
Phenom

1. you have differnt userdefined attributes e.g.

 

batchN and batch_N.

 

Please correct to batch_N for all MUs

 

2. Then add a method with the following code to the

 

entry method of the line object:

 

 

@.batch_N:=Batch_var;

Betreff: How to assigne a user defined attribute for all the MUs in one batch?

Valued Contributor
Valued Contributor

I corrected the BatchN and Batch_N. Now it's only BatchN for all MUs. And I added a method at the dismentalStation:

 

@.BatchN:=Batch_var;
Batch_var:=Batch_var+1;

 

This method was triggered at the Entrance or Exit under Controls. But I got an error message: Unknown: Unidentifier BatchN.

 

Please help.

 

Thank you

Steve

 

Betreff: How to assigne a user defined attribute for all the MUs in one batch?

Phenom
Phenom

Well, you didn't follow, what I posted you to do.

 

The (main) MUs entering the dismantle station and exiting to the drain1 do not have the user defined attribute

 

batchN !

 

Only the mus you dismantled from the main MU , which are leaving to the line.

 

Therefore the method was placed as line entry method.

 

 

Betreff: How to assigne a user defined attribute for all the MUs in one batch?

Valued Contributor
Valued Contributor

Now, it's working. I put th e Global Variable: Batch_var:=Batch_var+1 in the DismentalStation, as a user defined method. I followed your direction to put @.BatchN:=Batch_var at the Line method and triggered at the Exit. It works.

 

Thank you so much.

Steve

Betreff: How to assigne a user defined attribute for all the MUs in one batch?

Valued Contributor
Valued Contributor

Attached is the model. It works. Each MU got its batch number.

 

Since the two models will mix each other after the Cold Test due to the re-routs. I can use this batch number to re-sequence after Cold Test stations and make the down stream operation easier.

 

Thank you again.

Steve