Cancel
Showing results for 
Search instead for 
Did you mean: 

How to call 3 different entities separately into transporter.

Creator
Creator
Hi experts.

Hi have three source s with E1,E2,E3 entities.which goes in to buffer. I want to call E2 first from buffer to transporter to drain on track.


I really appreciate anyone send example on this in plant simulation.

Thanks in advance.

I am working on Plant simulation 12.
1 REPLY 1

Re: How to call 3 different entities separately into transporter.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Inventor,

I recommend to use the object Sorter. It is a buffer which sorts the part according to a certain sort criterion.

In the attached model the Source generates the sequence of part: E1, E2, E3, E1, E2, E3, E1, E2, ...

The MUs are equipped with a custom attribute customAttr of type integer.

The values of the MU-attribute are 1 for E2, 2 for E1 and 3 for E3.

Check the Sorter: Deactivate the check box Open Line. Run the simulation, activate the check box Open Line and start the simulation again. The object Line is filled. The first four MUs have the name "E2".

Regards,

Peter