Cancel
Showing results for 
Search instead for 
Did you mean: 

How to consider the OEE in simulation model

Creator
Creator

Dear Expert,

 

I want to know how to consider the OEE in simulation model? Set it as availability in Failure Tab?

2 REPLIES 2

Re: How to consider the OEE in simulation model

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The OEE is an outcome of the simulation run. If you drop a SingleProc onto a Chart object, you will see the development of the OEE statistics. The resulting OEE follows from the settings of the SingleProc itself and its interactions with its environment.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: How to consider the OEE in simulation model

Legend
Legend

You could also compare the ouput from the line with the target output, this will more or less be the OEE value for the line.

 

Simulated value = 75,6 pieces per hour

Target value = 100 pieces per hour

 

OEE for the line = 75,6/100 = 75,6% OEE