Cancel
Showing results for 
Search instead for 
Did you mean: 

How to deal with 2 PickandPlaces working together without colliding ?

Genius
Genius

Hello,everyone

 

I create a model about using 2 pickandplaces  to get parts from the same machine("M1").the model is posted in the attachment.

If there are no failures ,the  model can work smoothly, even so,I doubt there is something wrong in the logic of methods calling the PickandPlace . As is shown in the following picture.

01.JPG

 

In the failures mode,there are "Errors" happenning when you run the model(" robot_failure02").How to deal with this problem? As is shown in the following picture.

 

 

02.JPG

 

Looking forward to your directions!

Give my best regards to you!

1 REPLY

Re: How to deal with 2 PickandPlaces working together without colliding ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
since you move the empty pallet in the exit control of M1, you will have problems, if one robot gets failed during loading and the method is calling the second P&P to the empty pallet

try this as a condition:

while @.empty=false and not @.cont.move(PP01)

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net