Cancel
Showing results for 
Search instead for 
Did you mean: 

How to display the 3D-mu animation in the container?

Genius
Genius

 

Hello,everyone!

 

I create a new model in the attachment.the objects "m1","m2" are assemble machine. the "m1" assemble one part with one container. The "m2" assembles 4 mus from "m1"  with 1 container.  And I want to the part or mus to queue on the "Z" axes, so i reset the mu animation of container.

However ,when I runs the new model,the part or mus  cannot display on the container .As you can see in the  following picture with red marks.

Any help is great appreciated!

 

 

 

 

 

捕获.JPG

 

2 REPLIES
Highlighted

Betreff: How to display the 3D-mu animation in the container?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello MarkLee,

 

in te parameters of the assembly station you set 'delete MUs'. Therefore the MUs are deleted and only the container remains on the assembly station.

If you want to see the attached MUs, you have to set 'Attach MUs' as assembly mode.

 

Hope this helps.

 

Regards

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: How to display the 3D-mu animation in the container?

Genius
Genius
Hi,GG!
you're very nice,it works out.Thank you!