Cancel
Showing results for 
Search instead for 
Did you mean: 

How to generate x parts each day for a year?

Creator
Creator

Hi, 

I am trying to set up the source to set up 2 parts every day for 255 days but with the delivery table it gives me an error (A time specified has become negative). I don't understand why. 
For me it would be fine also to use a normal distribution where on average 2 parts per day are generated for 255 days or 365 days (it doesn't matter). 

Anyone knows how to do this? I can attach the model if needed. 

5 REPLIES

Re: How to generate x parts each day for a year?

Genius
Genius

I think a delivery table should work.  The DeliveryTime column should contain the overall simulation time of each creation of two parts.  For example:

 

1:00:00:00.0000

2:00:00:00.0000

3:00:00:00.0000

 

and so on for each of the 255 days.

 

 

Re: How to generate x parts each day for a year?

Creator
Creator

Yes it works now, I had a problem in a single process operation.
Do you know how to statistically distribute 20,000 objects over 255 days ? Instead of using a delivery table but maybe with a function.
Thanks 

Re: How to generate x parts each day for a year?

Genius
Genius

You could do this in an exit control on your Source.

 

Continue to use a delivery table to create one new MU for each of the 255 days.  Connect this Source to a Drain.

 

In the Source exit control, determine the number of parts needed for the day with a random distribution with a mean of 20,000/255 = 78.4, rounded to an integer.   Then in a for loop, use the create method to generate that number of MUs to a Buffer that connects to the rest of your model.

 

 

 

Re: How to generate x parts each day for a year?

Creator
Creator

Could you make a quick model example? I'm not so expert with this software and it looks quite complicate to me. 
Thanks in advance

Re: How to generate x parts each day for a year?

Genius
Genius

Here's an example model.  An MU exits the Source once each day per the Source delivery table.  In the exit control Method, a random number of copies of this MU is created.

 

This model is built in Plant Simualtion 13.