Cancel
Showing results for 
Search instead for 
Did you mean: 

How to implement dwell time with triangle distribution

Pioneer
Pioneer

Dear Plant Simulation Experts,

 

Thank you for your kind support.

 

I have a quesiton about dwell time in Buffer object.

 

In Buffer object, dwell time should be entered with only 1 const value.

 

But, I want to enter 3 values with triangluar distribution into dwell time, Buffer object.

 

In case of that, how can I do it ?

 

Thanks in advance.

 

4 REPLIES

Betreff: How to implement dwell time with triangle distribution

Gears Phenom Gears Phenom
Gears Phenom

Hi Beagle,

 

quick answer: Sorry, you can't Smiley Happy

 

The buffer has only a constant dwelling time. Else, with random dwelling times (such as triangular distr.) the MU's would be able to overtake themselves while they are in the buffer. That is not allowed/possible.

 

Is this what you actually want? So that the 1st MU stays 2min in the buffer, the next 2.5min and the 3rd MU only 1.5min? Then maybe the 3rd MU can leave the buffer before the 1st one is finished.

 

Regards,

Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: How to implement dwell time with triangle distribution

Pioneer
Pioneer

Dear Alex,

 

 

Thank you for your fast comment.

 

Maybe, I have misunderstood it wrongly.

 

Thank you for your instruction.

 

Thanks.

 

 

BR,

Beagle

Betreff: How to implement dwell time with triangle distribution

Siemens Phenom Siemens Phenom
Siemens Phenom

If you want the MUs to be able to overtake each other in a "buffer", you can use a ParallelProc and set a triangular distribution for the processing time of the ParallelProc. On the tab Statistics  of the ParallelProc you can se the Resource Type to "Storage", so that the time in the buffer is not statistically counted as "Production" time.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Betreff: How to implement dwell time with triangle distribution

Pioneer
Pioneer

Dear MichaelJoos,

 

 

Thank you for your comment.

 

Actually, What I want to know is that some area with the number of MUs which dwelled in the Buffer for 4 hours.

 

Then, If this dwell time is distributed with 3 ~ 5 hours, triangle distribution, of course this area with the number of MUs values will be changed and I want to know it.

 

That's why I am posting my quesion to this Forum.

 

Thanks and I will do it with your comment.

 

Thanks.

 

BR,

Beagle.