Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to model the sequence: If parking is full (cap:30), leave (drain), if not continue?

The capacity of the parking is 30. Before entering the customer checks whether there is a free parking space. If YES customer enters the parking lot, if NOT, he leaves (DRAIN).

 

HOW TO MODEL THIS SEQUENCE IN TECNOMATIX?

 

Thank you.

2 REPLIES 2

Re: How to model the sequence: If parking is full (cap:30), leave (drain), if not continue?

Phenom
Phenom

One way is to connect the "parking place" as successor 1

 

and the drain as successor 2

 

and set the predecessor exit strategy  as follows:

 

Unbenannt.PNG

Re: How to model the sequence: If parking is full (cap:30), leave (drain), if not continue?

Thank you Sir. 

I've modelled in this way. I've put FlowControl object and set Start at successor 1 as Exit Strategy.

 

SIM.JPG