Cancel
Showing results for 
Search instead for 
Did you mean: 

How to optimize the graphics

Creator
Creator

Hello everyone,

 

I have build the model in plant sim but it consist of to many high graphic robots and Object due to which the performance of Plant Sim has reduced. 

 

Do any one knows how to optimize the graphics ?

 

I have tried opening the 3D object in new 3D viewer window and then after selecting I right clicked the object but the optimize option is not there. Please refer the attached screen shot.

Screen Shot.png

 

So do any one know any other method to optimize the graphics?

 

Thank you,

Gopal Sharma

1 REPLY

Re: How to optimize the graphics

Siemens Phenom Siemens Phenom
Siemens Phenom

The built-in "Optimize graphic" function was a new feature in 11TR1. If I remember correctly (and the screenshot seems to confirm that), you're currently working on version 11.0.

If you have access to Teamcenter Visualization, you can simplify graphics there instead (or migrate to a newer Plant Simulation version, of course Smiley Happy).

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution