Cancel
Showing results for 
Search instead for 
Did you mean: 

How to program or set up a model about the time algorithms operation?

Creator
Creator
Hallo everyone !

I need to set up a order delivery model which should behave just in time or delayed. If the delivery is delayed, the arrival datetime should be later than the scheduled date time, it means :

Real arrival date time - scheduled date time= delivery time tolerance < 0

So I define the the delivery time to tolerance as , e.g. - 1day, which means "delayed", if the input is scheduled date as "12.Mar 2016", so the output , the real arrival date should be "11Mar 2016".

But it seems it doesn't work, the reason the plant simulation tool named is " the set-up date is negative" .

Is there someone who knows how to overcome this?

Thanks a lot in advance!

Best regards

J. Inkheart


1 REPLY 1

Re: How to program or set up a model about the time algorithms operation?

Siemens Phenom Siemens Phenom
Siemens Phenom

This should fit to your needs:

XXX.png

 

The attached spp shows all three cases that could happen.


Regards

Always consider using the AttributeExplorer!