Cancel
Showing results for 
Search instead for 
Did you mean: 

How to reduce a transporter speed constantly

Experimenter
Experimenter

Dear all,

 

is it possible to reduce the speed of a transporter constantly after every 10 meter on every path in a network?

For example: At the beginnig the speed of a transporter is 30 km/h. After 10 meter the speed reduces to 29 km/h. After another 10 meter the speed reduces to 28 km/h and so on.. So the speed at the end of way1 may be 20 km/h. After passing the single station he will drive on way2 and his speed "starts" at 20 km/h. After 10 meter the speed reduces to 19 km/h. After another 10 meter it reduces to 18 km/h and so on...

 

If anybody has an idea on how to fix my problem, please let me know.
Thank you for any suggestions!

 

Best regards,

JuliaB1

 

 

2 REPLIES 2

Re: How to reduce a transporter speed constantly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Julia,

you can use sensors at the ways: Click right onto the Way object and select Create Sensor.

When the transporter passes the sensor the assigned method is called:

You must set the speed of the transporter by the instruction

@.speed := 30/3.6

Note that the speed is measured in m/s. The shown instruction set the speed 30 km/h.

Please read also the documentation to the method  str_to_speed. Use the index.

Regards,

Peter

Re: How to reduce a transporter speed constantly

Experimenter
Experimenter

Hi Peter,

thank you for your answer!

Best regards,

Julia