Cancel
Showing results for 
Search instead for 
Did you mean: 

How to restore inheritance

Experimenter
Experimenter

Hello,

 

is it possible to restore an inheritance after cutting it or to define a new inheritance between to existing objects.

If yes how?

 

Regards, Tobias

 

 

3 REPLIES

Re: How to restore inheritance

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For me it is not clear, what you want to do.

 

for attribute values: click on the orange square --> Apply (should be green than)

 

For objects you cannot "select" a new parent class.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: How to restore inheritance

Siemens Phenom Siemens Phenom
Siemens Phenom

There's a functionality called Replace Class. Usually it's used to change a class of an instance (i.e. change SingpleProc to ParallelProc without replacing object and redefining attirbutes). To use it you need to drag and drop new class object to the target object with ALT key pressed.

 

Not sure that it's exactly what you need, but you can try.

 

Scenario is the following

1) Create .Userobjects.SPOrigin - by duplication of SingleProc class

2) Derive .Userobjects.SPDerived from SPOrigin

3) Insert SPDerived instance to the frame.

 

now inheritance looks like SPOrigin --> SPDerived --> .Models.Frame.SPDerived

 

4) Cut inheritance for .Userobjects.SPDerived

 

Now you can Drag'n'drop SPOrigin to SPDerived with ALT key pressed. But that would remove SPDerived object and inheritance would look like

SPOrigin --> .Models.Frame.SPDerived

 

What you can do, derive one more class SPDerivedNew from SPOrigin. And then drag'n'drop SPDerivedNew to SPDerived. After that inheritance would be 

SPOrigin --> SPDerivedNew --> .Models.Frame.SPDerived

Regards, Vladimir.

Re: How to restore inheritance

Legend
Legend

Hello!

 

I was wondering if something similar can be done for MUs. I created some MUs and later realised that it would be better to create a class and derive them from it because they share some properties.

 

I have been trying but I have not been successful. Any help is appreciated. 

 

Thanks..

Sanchay