Cancel
Showing results for 
Search instead for 
Did you mean: 

How to show LED indicator in the frame ?

Hello All,

 

Can anybody help me with the showing of LED outside of the frame. I am using a frame with a parallel proc inside it. 

I want to show the LED indicator on the frame as it is seen on the parallel proc.

But not able to find an option to do that

anyone with any idea?

1 REPLY 1

Re: How to show LED indicator in the frame ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
you can use the displayPanel of the frame, there is one option LED, just set the right attributes (resWorking, failed, paused..) and the right colors
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net