Cancel
Showing results for 
Search instead for 
Did you mean: 

How to show a simulation time of last entity exit

Experimenter
Experimenter

Hi,

I would like to ask if it possible to show simulation time when last entities exit from the buffer. I have 3 enties generates through percentage. Each one has their own buffer before drain and i want to display simulation time of when entitie left buffer. 

2 REPLIES 2

Re: How to show a simulation time of last entity exit

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello StefaM,

 

I recommend to equip the Buffer objects with an user defined attribute lastExitTime of type time.

The rear triggered exit control does not need a move instruction. The MU is moved at this moment.

The code of the exit control is

?.lastExitTime := EventController.simTime

This value can be displayed as a Display Panel, which can be defined via the context menu of the Buffer object.

You can do it in the class of the buffers:

.MaterialFlow.Buffer.

 

Regards,

Peter

 

Highlighted

Re: How to show a simulation time of last entity exit

Experimenter
Experimenter

Thanks for your recommendation it worked now.