12-29-2016 05:42 AM
Hello all,
I have a problem with the Warehousing and Logistics Library.
When I try to import an excel file in the "Data Interface" of the Warehouse Manager, the following windows opens with a red marked line:
I am using Tecnomatrix Plant Simulation 13.
Can anyone help here?
Thank you,
Julian
01-03-2017 08:42 AM
You have cut the failure message in the bottom line of the debugger window. So I can just guess the probably opened xlsx-file has caused this failure. Anyway this should not happen and should be covered by a failure handler.