Cancel
Showing results for 
Search instead for 
Did you mean: 

Importing DWG

Experimenter
Experimenter

Hi!

 

I'm trying to import a 3D dwg-file into my factory (it's a robot). When I try with "Import graphics >> file.dwg" it just creates a rectangle on the floor; if I choose default (Internal) or deco(external) dosen't seem to make any difference. Is there a simple way to performe this task? or is it easier to convert the file to something else?

dwgImport.png

Thank you in advance!

1 REPLY 1

Re: Importing DWG

Siemens Phenom Siemens Phenom
Siemens Phenom

Importing DWGs or DXFs into Plant Simulation only imports layout files meaning that a plate as you see is imported. The use case for this is the overall construction layout of an entire plant, e.g.

To import the actual geometry, you need to convert the DWG into another suitable format. For a list of suitable formats, open the file format selection of the Import Graphic file selection dialog. Jt as our native format is of course supported, as well as a couple of other formats, depending on your particular Plant Simulation version. Parasolid files always seem to be a good choice to me (if Jt is not available in your source application, that is).

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution